Answer question
Why the analog values in the CM30 Effected when usind the digital inputs?
Greetings
I do using the ABB CM30 controller in an application that i use two analog input channel each for a separate application
I do use digital inputs (Two) as an interlock per channel
event think i working correctly till the interlock occur
the values( the analog values) that the CM30 read are effected even if i have one digital input activated
I do read the values of the analog inputs in the diagnostic window , that values are effected very bad if the interlock occur
Kindky advice