Answer question
MMS Communication
MMS Communication to be established between two controller with diffrent series of IP address. One Controller is having IP address 172.16.1.61(5SP2 Version) and other controller is having IP address 172.16.88.151(5.1 Revd).
Is it possible to establish MMS Communciation between these two controller with some settings change in RNRP.