Answer question
Determine which graphic is loaded in the onload event of workplace panel layout
I need to determine which graphic is loaded by using the javascript onload event for the workplace panel layout. I can successfully get the onload event to fire for a pane, but so far I have not been able to determine the content that gets loaded to the pane. My end goal is to set the panel sizes based on which graphic is loaded, which I can do via javascript to the cols property of the panel.