Answer question
Detect Operator Workplace disconnection in AC800m
When there is no connection between the operator workplace and the controller then the controller must be able to detect this.
When the operator is blind, red crosses on screen. Then the controller must shutdown the installation.
For instance if OPC services are not running or if no operator is alive.
Is there some kind of watchdog to dectect this in the controller ?