Answer question
Network Configuration - 800xa 5.1 FP4
As part of our network switch upgrade we are having problems with secondary network.
We have isolated and checked each individual cable on both primary and secondary switch the cables are landed in the right place.
Now what we observed is, all the computers are showing a connectivity on primary network with "domain.local" name on it but the secondary shows "unspecified network" (RNRP shows connectivity down).
When we unplug the cable or disable the primary adapter, the secondary network get connected and shows "domain.local" but no connectivity.
On the other hand plugging the cable back or enabling the primary adapter after identifying it shows "unspecified network", then i have to disable the secondary adapter to get connectivity on the primary.
Any valuable suggestion would be appreciated.