Answer question
IEC60870 Station Settings
Please find the attached Architecture as per attached architecture we are able to receive data at RTU560 and from RTU560 to IEC101 Master Simulator. But when we remove the Simulator and connect to Siemens Module we are not able to read the signals.
my doudt is in attached file IEC60870_PARTNER_STATION the link address is '0' and partner common address is '356'. if you see in IEC60870_Partner_pg2 the common address is '16228'.
should the partner common address in IEC60870_PARTNER_STATION and IEC60870_Partner_pg2 common address shall be same or i doesnt matter.
IN RTU560 Programming the link address is '1' and common address is '16228'.
i used same link and common address in simulator its is working and communicating.
Can any one answer why RTU560 is not communicating with Siemens but able to communicated with simulators.