Answer question
AC500 (Automation Builder) Profinet Commincation error with Balluf BTL7-V50T SensorSa
Hello,
i am working on ABB AC500 (PM595-4ETH) on Automation Builder, i have to connect the AC500 PLC with the Balluf Sensor BTL7-V50T Via Profinet Communication, i have downloaded the BTL7-V50T Balluf GSDML File from Balluf Site and successfully installed GSDML file in ABB Automation Builder, but after add the BTL7-V50T in Hardware tree and download the program in PLC, Profinet communication goes Offline.
i am using the IO Card (PNIO-CI501) on Profinet Protocol that card working fine, but when i add the BTL7-V50T in hardware tree all communcaiton Goes off. kindly see attached documnent.
Kindly resolve this issue ASAP.
Regards,
M.Faisal