Answer question
How do I prevent the Windows Taskbar from showing up?
System:
- Win 7, 32-Bit, SP1
- Compact HMI800 V5.1
- 2 monitors
Configuration:
- The HMI800 application is running on one monitor, another application on the other
monitor.
- The monitor with the HMI800 application is the main display (i.e. holding the Windows
Taskbar).
- The Windows Taskbar is configured as 'autohide' and 'locked'.
- The HMI800 application is running in full screen mode (Operator Workplace Mode).
Problem:
When I operate the non-HMI800 application (means clicking somewhere on it) and then move the mouse back to my HMI800 application and move the mouse down to the bottom, the Windows Taskbar shows up unintenionally, see attached screenshot.
As long as I just operate the HMI800 application, the Windows Taskbar never shows up as it is supposed to be.
How do I prevent the Windows taskbar from showing up in this case?
Thanks for answering this question.