Answer question
Documentation on FPBA-01 configuration
Using ABB 800xA version 5.1, we have several new motors with FPBA-01 Profibus adapters, that should be connected to an AC800M through a CI854 card. The FPBA and PPO are inserted into the hardware structure.
In the Control Builder "Help Topics", only NPBA and RPBA adapters are described.
I assume FPBA can be used with AC800M, since it can be created in the hardware structure. Anyone have a link to a document or manual with description of the Control Builder configuration parameters for the FPBA-01 adapter?