Answer question
No mapping between accountnames and security ids...
Hello,
I am going to be crazy soon.
Have installed 800xA for more then 10years and some times I have got the error "no mapping between accounts and security IDS was done" when I am installing a domain computer. It is in the configuration wizard when it should setup windows users. Earlier I have made some small changes, or reinstalled windows and got it working.
But, now I am stuck. I have reinstalled 20 times, reinstalled domain controllers, tested differens domain raising levels and so on...
What is the background to this error?? The 800xA version is 5.1 64-bit, the operatingsystem i am running is Server 2008R2 Sp1 Enterprise.
I would really appreciate i fast answer because i have to have the system reade on monday, a new domain with three DC and around 10 800xA nodes. Then connect to a newer multisystem....
Please give me some hints..
Best Regards // Mattias