Answer question
FlexIO Allen Bradley and AC800M EthernetIP communication issues.
Hello, Everybody!
We are working in a project using Ethernet IP communication trough FlexIO Modules and CI873 communication interface.
After some initial issues regarding EDS file integration, we got a functional hwd files.
However, there is some abnormal situation. The commands from/to IOcards works propperly only when we have DI card in the end of the distribution. Example, if we put a DI card in the first psition, all the DO an AO modules don´t work anymore, even doing a cold reset to AC800M controller.
The Allen Bradley Hardware used is:
EtherNetIP Adapter 1794
1794-IB32 DI
1794-OW8 DO
1794-OF8IH AO
1794-IF8IH AI
We are using 800xA 5.1 FP4 rev. E
Someone has this kind of problem?
Thanks in advance!