Answer question
Known Software Errors in PPA 2.1/2
Problem:Solution
- The error will be corrected in the next revision.
[ref 3BSE029867D0018 VASMASOITA0864 ]
- Known Software Errors in PPA 2.1/2
If a trend display is brought up with a time scope that matches an hierarchical log, the trend will get its interactive data from that log as well. As a result of that, the trace will be delayed more than desired. For this to happen the intervals must be of certain values. E.g. with a time scope of 6h and a signal logged at 5s, 15s, and 1 min, the trace could be up to 3-4 minutes behind.
- Article imported from the previous version of KnowledgeBank