Answer question
A random value was placed into the LKP Result
Problem:Solution
- This problem was introduced when the LKP FCM (TABL_FCM) object was enhanced.
This problem was introduced when the LKP FCM (TABL_FCM) object was enhanced with the BP_SET and BP_TABLE attributes. Now when writing though OMF (i.e. Unix Put Value or Operate IT B FCM display). The proper value is written to LKP Result. This is fixed as part of the System Services Fixes for Version 3.3/1 fixes. Click Here for the Instructions.
- Random value was placed into the LKP Result
A random value was placed into the LKP Result when writing through OMF (i.e. Unix Put Value or Operate IT B FCM display).
- Article imported from the previous version of KnowledgeBank