Answer question
Ethernet/IP Communications between AB ControlLogix and ABB AC 800 Controller
Hello,
We will be attempting to establish Ethernet/IP communications between a Rockwell ControlLogix Processor and an ABB AC 800 series controller. The communications will be initiated in the ControlLogix environment. Is there a standard method to established communications, over Ethernet/IP, such as “Assembly/Instance” Connections (done with ABB Drives) or MSG Instruction type etc?