Answer question
IAC communication between different subnet 800xA Systems
We have a case where we have 800xA systems (V5.1) with different IP series ( Area 4 and Area 20 for system 1 and system 2 respectively) and controller series also in different series ( area 21 and area 20)
as per RNRP routing its possible to have an IAC-Communication variable interface between two controllers of the different system if the Client-server network is connected,
We are planning to have one additional network card with network area 4 in system 2 and communicate with System 1, this way now AS and CS servers are connected between Syst 1 and Syst 2, will the RNRP route IAC communication between controllers? or is there any better workaround?
as per RNRP routing its possible to have an IAC-Communication variable interface between two controllers of the different system if the Client-server network is connected,
We are planning to have one additional network card with network area 4 in system 2 and communicate with System 1, this way now AS and CS servers are connected between Syst 1 and Syst 2, will the RNRP route IAC communication between controllers? or is there any better workaround?