Answer question
Modbus TCP to OPC
Dear Sir,
I am using an Energy Analyzer QA/S 4.64.1
Connections to the energy analyzer and energy meters are connected and I'm getting values of those meters
As this Energy analyzer having Modbus TCP for data sharing it should be possible to connect to an OPC which having Modbus TCP driver in it
In my case, I'm using Kepware as OPC. And I have provided the correct IP address for the device and communication is fine over there. But while I'm trying to capture those values using the TCP register address which is given by the Analyzer it always showing the maximum value. If the register is configured as a word it shows 65355 and while with Dword it shows the maximum value, not the actual value.
I have attached the screen snap of OPC Quick Client and Energy analyzer Data sharing also the attached the note which shows the exact details about the TCP register
I didn't get what I have done wrong over there
If you can help me out to sort out the issue that will be very helpful
WBR
Amal