Answer question
Hanging / Lingering / Ghost IEC61850 alarms in 800xA Alarm List
I am experiencing lingering / ghost IEC61850 alarms in 800xA Alarm List. New alarms are generating and getting acknowledged as normal but the alarms are shown in the attachment stays there regardless of the actual state of the signal. I can delete these alarms but when one of our redundant servers are restarted or shut down then these alarms with old timestamps shows up again in the alarm list (in 800xA) in RTN state. So these alarms actually exist in the system and need to be deleted from the location where they are stored, but I don't know that location :)
Same problem with many objects. How can we get rid of them?
Same problem with many objects. How can we get rid of them?