Answer question
View Selection Buttons on Faceplates
We recently upgraded from 800xA Version 5.1 Rev D to V6.1. On our V5.1D system: If we have a Faceplate opened with only the Faceplate view available (two dots only), then open a faceplate with all three faceplate views available, only the two dots will appear. The one dot and three dot options will not appear. We were told this would be fixed on V6.1 (release notes have a number of 800xASYS-OL-5140-076 - please see below), but our V6.1 system behaves the same as our V5.1D. On other V6.1 systems the issue appears to be fixed - ABB has tried this on some of there V6.1 systems. Where would I go to fix this? Please see the attached released notes that indicates it will be fixed.