Answer question
Is there any Scan difference between Control Module and Function Block ?
Control modules are having default input Pins of 4 or 16.
Where as Function Block is user defined for Input Pins.
Will this affect the Cyclic Load on the Controller ?
Ex: I have 5 inputs that are connected to an AND Block.
In case of Control Module I need to use 16 Pin Block, but where as in Function Block I can define 5 pin Input and connect.
Where as Function Block is user defined for Input Pins.
Will this affect the Cyclic Load on the Controller ?
Ex: I have 5 inputs that are connected to an AND Block.
In case of Control Module I need to use 16 Pin Block, but where as in Function Block I can define 5 pin Input and connect.