Answer question
Speed shootup in jogging mode of ACS800 multidrive
We have two drives D24 and D25. D24 is master and D25 is follower. When i press jog forward of this group through GOP2000. Drive speed got high up to 138 to 140 rpm while its set point is 15 rpm.i have changed RDCU. Issue was not repeated but after one day it get started again. Kindly guide me what is the issue? It is hardware related issue or software related issue. I have replaced d24 with D25 but issue is persisting in D24