Answer question
Configure ViewClass to open Overlaps with zoom (150%)
I want to configure , on one of the workplaces, that all Overlaps open with a Zoom of 150% by default (this is because of the different resolutions of the Displays used).
I guess from looking at the pre-defined workplaces it should be possible with ViewClassMapping and different Viewclasses to define this.
From the existing System i see configured in the Viewclass it's possible to have a fixed size (Width/Height in Pixel) or define in the Override General Properties ScaleLayout = resizetofit then Overlaps will open with pre-configured size. Is there any way to define the Scaling to resize to a pre-defined Zoom Level (instead of 100%)?
Does someone have a description of all the General Properties possible in ViewClass?