Answer question
MB300 Uploader for Ac400 Connect
Please could you support in the following question?
Customer has a system installed and they are close to reach the tag license limit. They need to add some objects ,but they would need to delete some objects which they will no need to see from 800xA. Then we would add some additional objects like 10 or more , we would need to run MB300 Uploader to add them to 800xA system. But it would add all the objects again, an we would exceed the tag count. The question, if we run MB300 Uploader but from buttons add /remove we could selectively choose just the objects required ,because the blank option means everything is uploaded from controller , if we click on Add or remove buttons, does the system show all the objects belong to the specific controller and removing some of them y just keep the additional objects on the list we just would upload the additional objects from controllers to 800xA system.
Thanks for your support
Best Regards
Ricardo
Customer has a system installed and they are close to reach the tag license limit. They need to add some objects ,but they would need to delete some objects which they will no need to see from 800xA. Then we would add some additional objects like 10 or more , we would need to run MB300 Uploader to add them to 800xA system. But it would add all the objects again, an we would exceed the tag count. The question, if we run MB300 Uploader but from buttons add /remove we could selectively choose just the objects required ,because the blank option means everything is uploaded from controller , if we click on Add or remove buttons, does the system show all the objects belong to the specific controller and removing some of them y just keep the additional objects on the list we just would upload the additional objects from controllers to 800xA system.
Thanks for your support
Best Regards
Ricardo