Answer question
AC800M IP Address
I have an older 800xA System on some mobile equipment that through out its life has been shut down put on shore power many times, batteries have died in the cold and lost the program in the controller and I was always able to install a new battery and upload the program into the controller no problem and didn't have to do any more than that. The other day I turned a system back on that has been working recently and was plugged into shore power and when I turned the control system on I got an error from windows saying I had IP address that are the same on the network, to make it short and sweet the IP address had changed in the controller and I have never had an IP address just change on it's own to the same address as the standalone engineering station in the controller. Does anyone know how this can be possible?