Answer question
What is the latest ABB verified cumulative security update for Win10 LTSB2016 and Server 2016 (5th April 2019)
I'm setting up new 800xA system (6.0.3.2).
I have installed Windows 10 Enterprise LTSB 2016 (1607) on the clients, and Windows Server 2016 on the servers. I'm looking to install the latest cumulative security update from Microsoft before I start the Node Prep.
The table for Win10 1607 updates published by Microsoft (which covers both Win10 LTSB 2016 and Server 2016) shows the most recent KBs (below, I have listed the most recent first), and I've added the comment for each taken from the 3BSE041902_OO ABB Third Party Update Validation document by ABB (20th March 2019):
Can someone confirm that these are the correct cumulative security updates for me to use, and that none of the newer updates are applicable for use with 800xA?
I have installed Windows 10 Enterprise LTSB 2016 (1607) on the clients, and Windows Server 2016 on the servers. I'm looking to install the latest cumulative security update from Microsoft before I start the Node Prep.
The table for Win10 1607 updates published by Microsoft (which covers both Win10 LTSB 2016 and Server 2016) shows the most recent KBs (below, I have listed the most recent first), and I've added the comment for each taken from the 3BSE041902_OO ABB Third Party Update Validation document by ABB (20th March 2019):
- KB4489889 (19/03/2010) - <Not tested by ABB at time of publishing validation document>
- KB4489882 (12/3/2019) - "is not qualified for 800xA due to Microsoft known issues"
- KB4487006 (19/2/2019) - "Not applicable as superseded by 4489882"
- KB4487026 (12/2/2019) - "is not qualified for 800xA due to Microsoft updated known issues"
- KB4480977 (17/1/2019) - <not mentioned in ABB validation document>
- KB4480961 (8/1/2019) - "Not qualified for 800xA. This update has known issues from Microsoft. (Our test environment foes not provide conditions that our customer may have for symptoms of issues from Microsoft.)"
- KB4483229 (19/12/2018) - "Released on Dec 19th 2019. Superseded updates have been qualified"
- KB4471321 (11/12/2018) - "Not approved for 800xA due to potential impact of known issues reported in Microsoft KB"
- KB4478877 (3/12/2018) - <not mentioned in ABB validation document>
- KB4467684 (27/11/2018) - <not mentioned in ABB validation document>
- KB4467691 (13/11/2018) - "Not approved on 800xA on Windows Server 2016 due to potential impact of known issues reported in Microsoft KB"
- KB4462928 (18/10/2018) - <not mentioned in ABB validation document>
- KB4462917 (9/10/2018) - "Prerequisite KB4132216 [an SSU update] is qualified"
- KB4457127 (20/9/2018) - <not mentioned in ABB validation document>
- KB4457131 (11/9/2018) - Approved
- Server 2016 - KB4457131 from the 11th of September 2018. Now nearly 7 months old.
- Windows 10 LTSB 2016 - KB4467691 from the 13th of November 2018. Now nearly 5 months old.
Can someone confirm that these are the correct cumulative security updates for me to use, and that none of the newer updates are applicable for use with 800xA?