Answer question
Why aren't the tabbed workplace buttons displaying on the client when they display on server?
I have a single-screen tabbed workplace set up for a two-node system (1 AS/CS and 1 client). I can open the operator workplace on the server and the tabbed workplace buttons display as expected. However, when I open the workplace on the client, the buttons are not displayed and there is a message that the base pane cannot be located.