Answer question
Freelance User Function Block: how to create instance out of User-Defined Object Type in 800xA
I have created in CBF an User Function Block (UFB, Name Ilock), then an instance "tesIlock" of it and exported the *.ple-File via projectmanager.
In 800xA I have created under Object Type Struct->Control System->Freelance 800F Connect->User Defined Function Blocks an object Type "U.Ilock" (from the U.Template).
If I upload now the ple-Confi there is no instance object of "tesIlock" created wihtin the control struct.
What do I have to perform to get instances of my new UBF "Ilock" and object type "U.Ilock" while uploading the ple-File?
Do I have to tell "AC800F Uploader" which UFBs to create objects from?
Thx in advance.