Answer question
System Extension Load on system that is UP
Hello!
Can I load a system extension while the system is running (in this case PLC connect) or do I need to stop the 800xA system?
Also do I need to install PLC connect on all nodes? I have installed it on 1 AS as of now.
800xA 5.1 is the version we have.
Thanks in Advance!
/Trinity
Can I load a system extension while the system is running (in this case PLC connect) or do I need to stop the 800xA system?
Also do I need to install PLC connect on all nodes? I have installed it on 1 AS as of now.
800xA 5.1 is the version we have.
Thanks in Advance!
/Trinity