Answer question
CI867 and Modbus RTU Slave on daisy chain
I am using CI867 Module as Modbus Master module for polling the data at controller side.
We are using Moxa Gateway for Modbus RTU devices, there are multiple serial slaves that are communicating on daisy chain. These slave are connected to a port in daisy-chain(Multi-drop) to a converter on RS-485 interface.
Please tell how to configure the Modbus slave in this case at controller end.
Under Gateway how to define the slave ID. How slave ID is different w.r.t. Slave Position?
Regards