Answer question
Can we run a motor with nominal voltage 230 V, whereas the VFD operated with 400 V incoming?
I have a motor with following ratings-
In Delta 230V, 4KW, 13.9amp, 1454rpm, 50 Hz
In Star 400V, 4KW, 7.9amp, 1453rpm, 50Hz
and Drive is ACS850-04-025A-5+J400, hence incoming supply is 400V.
I want to start the drive in Delta connection is it possible?
And if possible Is there some advantage to run the motor in Star?
For example better control in Star.
In Delta 230V, 4KW, 13.9amp, 1454rpm, 50 Hz
In Star 400V, 4KW, 7.9amp, 1453rpm, 50Hz
and Drive is ACS850-04-025A-5+J400, hence incoming supply is 400V.
I want to start the drive in Delta connection is it possible?
And if possible Is there some advantage to run the motor in Star?
For example better control in Star.