Answer question
CI867 communication with slave device on multi drop?
Hi,
Can we connect the CI867 Modbus TCP slaves on multi drop? Refer to attached image.
In our case around 10 AC500 PLC's are connected to one CI867 in multi drop.
Communication with slaves are not continuous, fluctuation of data is observed.
Q: can we use the above configuration for CI867 TCP communication?
Any specific settings need to be done at CI867 card level?
Thanks
Can we connect the CI867 Modbus TCP slaves on multi drop? Refer to attached image.

In our case around 10 AC500 PLC's are connected to one CI867 in multi drop.
Communication with slaves are not continuous, fluctuation of data is observed.
Q: can we use the above configuration for CI867 TCP communication?
Any specific settings need to be done at CI867 card level?
Thanks