Answer question
Store a program into a SD Card AC500-eco
Hello, I have made a project with a PM554-TP-ETH and I want to store it into a brand new MC502 card. I have followed the process that appears in the ppt about the SD card but when I write the command sdappl the process fails and at the bottom of the screen appears the following text "#152310029: '- 1970-01-01 00:01:28 E4: SD Card 'Failed to copy boot project to SD Card -> Check SD Card for free space.
As I have said the SD Card is new and it has only the folders structure and the ini file on it. It is a 2 Gb SD Card, it has more than 1 Gb of space free and the program is very simple just a few lines of ladder code. I have tried to use different versions of the firmware and also tried to force the values of the parameters FunctionOfCard and UserProgram in the SDCARD.ini file but the result is always the same.
Could you give me any idea or solution? Thank you in advance.
Regards
As I have said the SD Card is new and it has only the folders structure and the ini file on it. It is a 2 Gb SD Card, it has more than 1 Gb of space free and the program is very simple just a few lines of ladder code. I have tried to use different versions of the firmware and also tried to force the values of the parameters FunctionOfCard and UserProgram in the SDCARD.ini file but the result is always the same.
Could you give me any idea or solution? Thank you in advance.
Regards