Answer question
Is is possible to develop FBD logic in Single control modules for SIL 3 applications?
I have been working on making a SIL 3 application and after being made familiar with the limitation of the soft controller of not being able to connect more than 8 applications I have to re-organize my code.
I need a suggestion of how to re-order my code; since it is not possible to insert sub-levels in programs, I was considering of making layers of single control modules and using its editor to develop FBD logic?
Please advise if this is a viable option or should i stick to programs?