Answer question
AC800M - MotorUni motor block
Good day,
Im using the MotorUni block in my program. I need some clarity on the connections made to the block.
Please check if my assumptions are correct:
- If i connect a signal to the "SetAuto" the motor is in auto mode??
- Now to start the motor in auto, "AutoCMD1" must be 1??
- To stop the motor, "AutoCMD0" must be = 1 and "AutoCMD1" = 0??
Now my next question is, how do i start the motor in manual??
Which inputs do i use to start & stop the motor??
Also, which input do i use for "Local" mode, and do i need to use the same inputs (Start & Stop) as manual??
Please assist.
Thank you.
Kind regards,