Answer question
PM583-ETH Profibus Communication with Third party device integration
Hi All,
I am new to ABB PLC programing. for my project using PM583-ETH and CM572-DP module. in Feild Bernard control MOV is available, so that i have added Bernard *.GSD file in Control builder Plus V 2.3.0 tools/Device Repository.
When I add profibus slave device(Bernard controls Intelli+2801) and i am getting error message" Slave:[ERROR] Intellibus_2_PDP_SINGLE [AC500_PM583_ETH: Communication_modules: CM572_DP: CM572_Master]: The slave : Intellibus_2_PDP_SINGLE should have at least one communication module!".
Even I cant I/O Map in offline. Pls let me know IO Mapping either canbe done offline or online, the way am I doing right? or I have to use SYSCON software.
Pls share any documents or videos or sample program.
Thanks alot...........