Answer question
ABB MB300e two networks connectivity through a Multiplexer
This time we are connecting the two ABB MB300E networks through a Multiplexer using two different Interfaces (one for each network), to provide two redundant networks over the radio . The MUX output is an E1 port (E1 is about 32 channels , to segregate all of its traffic) that is directly connected to 1+1 HSB radio. This is the basis of our old design and i see this as a very good architecture to follow up with the two cited netwoks we are talking about, because i think the MUX is doing a great job here , don't you think so?
Thansks for all of you for participating in this.