Answer question
One CI867 as Master and Slave
I have a requirement in wherein two 3rd party package interfaces are connected to the same AC800M with a single CI867. One of the interface has ABB system as the master and the other needs ABB system as slave. Is it possible to have the same CI867 act as master for one package and slave for another?