Answer question
MSI Upload error i.e E_AFW_OT_RULE_CONSTRAINT(0x8abb0a63) while uplading.
Hi I am trying to append (Reload modified graphics displays) few graphics displays to existing MIS configuration in a ABB800xA System SV5.1-0 with VB Graphics. While uplading I am getting two errors.
1.Error - The 'Cogen' object is not allowed as a child to object 'Renukoot' in structure Object Type Structure (type 'Object Type Group').
2.Error - E_AFW_OT_RULE_CONSTRAINT(0x8abb0a63) Object type rule constraint.
Also while checking the consistancy of MSI in object type structure we got the first error mentioned above. i.e
1.Error - The 'Cogen' object is not allowed as a child to object 'Renukoot' in structure Object Type Structure (type 'Object Type Group').
Heare 'Cogen' is an application name.
Kindly let me know where these rules are configured? How to relese the object from these rule constraint.
Br/PK J