Answer question
IEC61850 Upload error
Hej!
Ställde denna fråga på forumet men blir inte riktigt klok på svaret.
Skriver till lite info här före.
Vi har bef 4st instanser i drift som ligger installerade på en kombinerad AS/CS.
Ska nu drifta ett femte ställverk. Ny PC (icke xA-nod) är skapad för denna femte OPC-server eftersom det endast kan vara 4st på en xA-nod. Rätt?
Eller kan det endast vara 4st totalt mot samma AS-server?
Ny Service Provider skapad som kör på den kombinerade AS/CS-noden men med sökväg till den externa nya OPC-servern (Remote OPC Node) som ligger på en egen PC. Rätt?
Här funkar det fint att browsa och välja OPC DA-servern i den externa PC:n.
Denna Service Provider får vi till att gå upp i Service.
När vi sedan försöker göra Upload på SCD-filen händer det nedan.
Har du någon ide?
---
In English:
We have four operating instances installed on a combined AS / CS.
Will now operate a fifth switchgear. New PC (non xA node) is created for this fifth OPC server because it can only be 4st on an xA node. Right?
Or can it only be 4p total against the same AS server?
New Service Provider created as running on the combined AS / CS node but with path to the remote new OPC (Remote OPC) server (OPC) server located on its own PC. Right?
Here it works well to browse and select the OPC DA server on the external PC.
This Service Provider tells us to go to Service.
When we then try to make upload to the SCD file, it happens below.
Do you have any ideas?
---
When trying to upload the scd file in Control Structure this error appears.
From the log:
Connecting to: IEC 61850 OP DA Server Instance[5] on the machine xxxxx
Connected to the OPC Server!
*
Starting Control Structure retrieve...........
Error: WA5\xxxxxxx
Error: Uploading failed, OPC Server is using different configuration
Error: Failed to do Control Structure retrieve
The upload operation has failed!
End log
We are using the same file when uploading in 800xA as we did when uploading in CET.
Anyone?
Or does anyone know who I should contact in this matter?
BR asp