Answer question
Printer problem with ABB 800xA System
We have large ABB 800xA setup with about 50 Controller, 04 AS/CS Server, 06 HMI and 01 ENG Station. The 50 controllers are evenly distrubuted among these 04 AS/CS Servers. We have 02 Printers connected on same network. We have dedicated switches for C-net(Controller Network) & P-net(Process Network).We are using Hirchmann 1040 Gigabyte Ethernet Switch.
When ever we are giving printer it is taking long time to print; somtimes it is not-at-all printing.
The IP address of Printer is as given below:
IP:172.16.4.92/Subnet: 255.0.0.0./Default Gateway is 172.16.4.92.
The IP Address of ENG Station is
IP:172.16.84.13/Subnet: 255.255.252.0.Default Gateway is -.-.-.-
For printer I Tried with Subnet of 255.255.252.0 but no use.
Please advice...
Also,Is it OK to configure ENG Station/HMI/Servers etc on network without Default Gateway?