Answer question
Freelance 2000 ver 3.2, Digivis communication with PS_2 aborted!
Hi!
Thanks for your replay about lateral communication error. It now works fine.
I have this even worse problem now after a power breakdown this weekend.
The Digivis-program on both my workstations, OS_1 and OS_2, have problem communicating with one of my PLC:s PS_2. Gives the error I wrote in the header.
No problem at all with PS_1.
If i Try to ping the PLC I get timeout in every fourth every sixth ping.
I have exchanged the coax cable and the terminate resistor.
I have also restarted the system and loaded the program with Load whole station.
The strange thing is that I can download program without any trouble.
What do you think? Any idea?
Is there some other way to make a reset on the CPU board?
Best Regard Anders