Answer question
Inherit Property Transfer Definition Aspect with Name Aspect as target aspect
I configured the Property Transfer Definition Aspect at an object in the Object Type Structure. I want to use the Property Transfer to overwrite the description of the Name Aspect by using an opctag of the Control Connection Aspect.
At the Object Type Definition Aspect I set "Inherit to all instances" for the Property Transfer Definition Aspect.
At the child object in the Control Structure the Property Transfer Definition Aspect was inherited but the field with the target aspect is empty.
Is it possible to inherit a Property Transfer Definition Aspect with name aspect as target aspect?
I know that the Name Aspect is gernerally not inherited but is there any other way to solve the problem?