Answer question
ABB Panel 800 PP877 ethernet / network settings
Cannot find any info about where to set speed(10/100) and simplex/duplex. Is there a default setting for this, or it is automatic sensing the switch settings(Switch are to be manually configured).
Can find info that different protocols can be selected, but no info abut what these protocols contains....
The ABB CoDeSys TTH driver supports three different protocol types:
1. Tpc/Ip Level2 Route
2. ABB Tcp/Ip Level2 Route AC
3. Tcp/Ip