Answer question
All scheduled jobs fail to run on any Scheduler Data Provider in the 800xA system
Problem:
No jobs will run on the system either using the Run Now button on the Scheduling Definition Aspect or when dispatched by the scheduler either with a periodic or cyclic time. And, if there are multiple Scheduler Service Providers in the system, jobs will not run on any of them. Also, you may find that the Run Now button will hang the Plant Explorer when used. Finally, the Test Action of the Context menu of the Action Aspect may work to run the defined action.
Symptoms:- Running report with Run now through Scheduling Definition Aspect freezes the Plant Explorer. CreateJobAspect failed! error in ABBScheduler.log file when attempting to run a report