Answer question
Warning in Maintenance Backup upplacedObjects.afw
During 800xa system backup there is warning [Warning] Unplaced objects exist, see "C:\BACKUP\Full_10June2019; 2019-06-10; 10-15\0_UnplacedObjects.afw".
We tried to the following steps below.
Escalate user to software developers group and then to create a new object in a structure that is not being used. Once there create a new object and to use the Set Guid button (this feature is specific to users within software developers). Once there, he pasted the GUID found from the unplacedobjects.afw and set the GUID. After the object was created the unplaced object was placed with all of its aspects. Was able to delete the aspects and then the object.
We tried to the following steps below.
Escalate user to software developers group and then to create a new object in a structure that is not being used. Once there create a new object and to use the Set Guid button (this feature is specific to users within software developers). Once there, he pasted the GUID found from the unplacedobjects.afw and set the GUID. After the object was created the unplaced object was placed with all of its aspects. Was able to delete the aspects and then the object.