Answer question
Harmony Composer 6.1 can't start
Hi!
I installed 2VAA003488_-_en_S__Engineering_Composer_Harmony_6.1.0.27.msi on Windows7SP1 32bit. During installation i get messages that following dll are not registered:
I installed 2VAA003488_-_en_S__Engineering_Composer_Harmony_6.1.0.27.msi on Windows7SP1 32bit. During installation i get messages that following dll are not registered:
ComposerConfigDataX.dll
ControllerConfigDataX.dll
ControllerConfigViewX.dll
DataBrowserX.dll
When i tried to register it manually, but can't did it.
When i tried run Composer i got error: "The program can't start because SplusCSA_API.dll is missing from your computer".
2VAA003489_-_en_S__Engineering_Composer_Harmony_API_3.2.0.34.msi was also installed.
How can i run Composer?