Answer question
Upgradation of PPA2.1-2 to 800xA4.1 with AC400 connect.
Hi,
I am trying to upgrade PPA 2.1-2 to 800xA 4.1 (Core 11b). I have installed 800xA 4.1 system with AC400 connect. Backup of PPA2.1-2 has been restored sucessfully.. but i am facing the problem with user rights.. because of this i am unable to add or create any new aspect in 800xA 4.1 system..can any one suggest me to solve this issue...?
Error Detail:-
I am trying to create an object in Maintenance structure--> Backup definations -->New object--> full backup definations - -> test
''Error: Access Denied Transaction cancelled, Failed to created object"
I tried to give user rights in Configuration wizard.
Administrator is already having all rights except administartor and operator.. but i tried to provide those rights also..
I failed to provide because of the following error:-
"Access Denied, No user cannot be added, change or deleted"