Answer question
What do the ConfigDataForSFC setting do?
I have read the Configuration manual
3BDS011222-510 B about the setting ConfigDataForSFC in Object Type Structure > Function Planning > Settings > Function Settings
On page 57.
"When the function setting ConfigDataForSFC is made True and all the logic is
created, the diagram reference name is shown in the action display."
I've built a sequence in Function Designer. I don't really understand what this setting will change. I'm using the SFC Viewer and clicking Step only show code which is a total disater like internal_linkA0E03CS etc. Will this setting change so that the diagram is opened instead?
Do I also have to change the Naming Conventing setting. Right now it's _FD but we use _FuD as diagram name ending.