PG2 Symbol and Tag Finder - Version 1.2 (.zip)
App id
20194818
File extension
.zip
File name
PG2Finder-Rev2.zip
Type
App
Version
1.2
File size
7.2 MB
Fixed a bug present in the 1.1 version. The bug was caused when the xgml files for the elements present in a graphic xgml were missing.
Version
Description
1.2 by damemk
Fixed a bug present in the 1.1 version. The bug was caused when the xgml files for the elements present in a graphic xgml were missing.
Added new functionality to the application to store information when graphical element is referencing another graphical element. Also, the output format contains information about the parent object that contains the referenced symbol. The format of the output file is based on the extension defined in the [Output Results] line (e.g. if xlsx then output is xlsx, if csv then csv). Also, two separate output files are created for Tag References and Symbol References)
This is a first version of standalone application that uses xgml files to determine on which graphics a particular PG2 Graphical Element is being used, as well as tags.
You must be logged in and have downloaded this app in order to post a review or rating. Login
Posted by
on
Dec 11, 2018 at 12:44 AM
by david.bravo-segovia Rank: 1018 on Jan 09, 2020 at 05:25 AM
I am triyng to get xml for many graphic displays with Graphic Xml tool and I get an error "Could not find file "AfwExpressionHandling.resources", how can I fix this?