Hardwired CB Open/Close Commands Interface on IEC61850 Faceplate - Version 1.0 (.pdf)
App id
20194779
File extension
.pdf
File name
10185_Hardwire-DO-command-Integration-in-IEC61850-MMS-Faceplates-on-800xA-System_APP_1-0.pdf
Type
App
Version
1.0
File size
3 MB
Normally on IEC61850 Integration, all signals are from IEC61850 OPC server on to HMI. If the Commands are to be via Hardwired then Integrating the HW Commands on to IEC61850 Faceplates is a challenge. This document gives a workflow to configure the same.
Version
Description
1.0 by Santhanam
Normally on IEC61850 Integration, all signals are from IEC61850 OPC server on to HMI. If the Commands are to be via Hardwired then Integrating the HW Commands on to IEC61850 Faceplates is a challenge. This document gives a workflow to configure the same.
You must be logged in and have downloaded this app in order to post a review or rating. Login
Posted by
on
Apr 12, 2018 at 07:15 AM
Posted by
on
Apr 11, 2018 at 08:12 AM
Posted by
on
Apr 11, 2018 at 08:11 AM
Posted by
on
Apr 11, 2018 at 08:11 AM
Posted by
on
Mar 24, 2017 at 08:25 PM
Posted by
on
Nov 12, 2016 at 03:40 AM