Extensible Parameter Function Blocks - Version 2.0 (.zip)
App id
20194775
File extension
.zip
File name
Extensible Parameter Function Blocks.zip
Type
App
Version
2.0
File size
19.6 KB
Version 2.0
- Added Important Notes and Instructions to the Code. PLEASE READ BEFORE USING THIS BLOCK!
- Added Compact Control Builder Source Code
- Compact Control Builder also includes a sample Application.
- 800xA Version 5.1 is used for Backwards Compatibility. For Version 6, import the library and upgrade it.
- Added Important Notes and Instructions to the Code. PLEASE READ BEFORE USING THIS BLOCK!
- Added Compact Control Builder Source Code
- Compact Control Builder also includes a sample Application.
- 800xA Version 5.1 is used for Backwards Compatibility. For Version 6, import the library and upgrade it.
Version
Description
2.0 by Rob Lyon
Version 2.0
- Added Important Notes and Instructions to the Code. PLEASE READ BEFORE USING THIS BLOCK!
- Added Compact Control Builder Source Code
- Compact Control Builder also includes a sample Application.
- 800xA Version 5.1 is used for Backwards Compatibility. For Version 6, import the library and upgrade it.
- Added Important Notes and Instructions to the Code. PLEASE READ BEFORE USING THIS BLOCK!
- Added Compact Control Builder Source Code
- Compact Control Builder also includes a sample Application.
- 800xA Version 5.1 is used for Backwards Compatibility. For Version 6, import the library and upgrade it.
Upgraded for System 800xA version 6.0.1, Feel free to review App and give us a feedback.
Extensible Parameters for User Defined Function Blocks
Extensible Parameters allow the programmer to use function blocks with a variable number of in, out or in/out parameters. The attached Template Library will allow programmers to create their own special function blocks which support extensible parameters.
How to Use...
- Import the attached AFW file to your system
- Include the ExtensibleTemplateLib in your project
- Copy the ExtensibleTemplate function block to your own library or projects
- Rename and edit as required.
Disclaimer: USE AT YOUR OWN RISK.
Extensible Parameters allow the programmer to use function blocks with a variable number of in, out or in/out parameters. The attached Template Library will allow programmers to create their own special function blocks which support extensible parameters.
How to Use...
- Import the attached AFW file to your system
- Include the ExtensibleTemplateLib in your project
- Copy the ExtensibleTemplate function block to your own library or projects
- Rename and edit as required.
Disclaimer: USE AT YOUR OWN RISK.
You must be logged in and have downloaded this app in order to post a review or rating. Login
by Neeraj Rank: 408 on Jan 19, 2021 at 09:08 PM
Hello sir,
could you provide extensible parameter template for version 5.0.1 CCB.
Thankyou.
by Rob Lyon Rank: 2 on Apr 03, 2019 at 03:14 PM
Please read and review the important instructions contained in the code. For further details read 3BSE047421D0222.
https://search-ext.abb.com/library/Download.aspx?DocumentID=3BSE047421D0222&LanguageCode=en&DocumentPartId=&Action=Launch